Tool/software:
Hi Teams,
I have one 6424 issue need you help:
A:
When i use 6424 to drive speaker (normal mode), 6424 can output audio single;
B:
When i use 6424 to drive a external amplifier (lineout mode), 6424 can not output audio single.Below are the setup codes of 6424.
I can not understand wether i set the value to register.
write to 0x6A ack data: 0x00 0x0F
write to 0x6A ack data: 0x01 0x32
write to 0x6A ack data: 0x02 0x60
write to 0x6A ack data: 0x03 0x44
write to 0x6A ack data: 0x04 0x00
write to 0x6A ack data: 0x05 0xFF
write to 0x6A ack data: 0x06 0xFF
write to 0x6A ack data: 0x07 0xFF
write to 0x6A ack data: 0x08 0xFF
write to 0x6A ack data: 0x09 0x02
write to 0x6A ack data: 0x0A 0x11
write to 0x6A ack data: 0x0B 0x11
write to 0x6A ack data: 0x14 0x00
write to 0x6A ack data: 0x15 0x00
write to 0x6A ack data: 0x16 0x00
write to 0x6A ack data: 0x21 0x00
write to 0x6A ack data: 0x22 0x01
write to 0x6A ack data: 0x23 0x14
write to 0x6A ack data: 0x24 0x00
write to 0x6A ack data: 0x25 0x00
write to 0x6A ack data: 0x26 0x40
write to 0x6A ack data: 0x28 0x0F
write to 0x6A ack data: 0x77 0x80
write to 0x6A ack data: 0x78 0x3F
write to 0x6A ack data: 0x79 0x00
Best Regards.
Hi,
What's load impedance of external AMP? I think TAS6424 is runing DC load diag and can not pass it, because the impedance if out of range(6K).
Hi Gong,
The external AMP 's Input impedance is 10KΩ, load impedance is 2Ω
Best Regard.
Hi Yunxuan
In that case, quite possible not able to pass DC load diag.
Have a try to set 0x81 into register 0x09, for line out using.
Hi Yunxuan
Please change 0x09 register value to 0x03 to disable auto DC load diag and lineout load diag if connect high impedance external AMP.
He Gong,
Thanks for your reply, but this issue still not fixed.
Can you give other suggestions?
If I set 0x03 into register 0x09, which parameter should I set into 0x00?
Best Regards.
Hi Yunxuan,
Sorry, please set register 0x09 to value 0x01, this is to disable auto DC load diag.
The root cause is external AMP impedance is out of range, so you can disable DC load diag.
Hi Gong,
When I set register 0x09 to value 0x01 or 0x03, which value should I set to register 0x00?
Best Regards.
Hi Yunxuan,
If you connect external AMP, please set to Lineout mode. so 0x00 register should be 0x0F.
Hi Gong,
Thanks for your reply.
I no sure whether 6424 was enter protection status, so how can I check this status?
May I use register 0x25?
Best Regards.
Hi Yunxuan
Register 0x0F could tell you the channel status.
And register 0x10 t0 0x13 could tell you if any Fault or Warning reported.