Hi,
I am trying to get the following scheme working in TAS3204:
TAS3204 has been configured to run in slave mode. I have generated the code (attached) using PurePath Studio GDE (version 1.88 build 5) and downloaded through I2C interface. The I2C download is fine since I am able to get audio out on DACs if I use signal generator blocks of TAS to produce the signal and output it to DACs instead of taking any input. But the above input-to-output bypass mode is not producing any signal at the output. We have probed the input and output pins of TAS, signal is seen entering the chip but nothing comes out at the output pins.
Is there any I2C register which can be read to get some information about what is going on inside TAS? I have checked the firmware download status register (I2C subaddr: 0x02), which didn't report any errors. Am I missing something?
Thanks in advance.
PS: I do not have an EVM board.