Hi,
I am following this sequence after hardware is initialized:
1. send 0x00 to register 0x1B.
2. send 0x00 to register 0x05.
Signals LRCLK (8kHz), SCLK(512kHz) and SDIN are connected at power-up.
1) If I follow the above sequence with MCLK(4.096MHz) also connected to TAS5713 at power-up, I get no output on PWM ( 0 V ) and there's PLL Error in Error register. I read 0x94 at Register 0x00.
2) If I follow the above sequence with MCLK(4.096 MHz) disconnected I don't have PLL error and PWM output is at 377.5kHz 50% duty cycle. If at this stage I apply MCLK(4.096MHz) to TAS5713, then PWM output becomes jittery and there's still no PLL Error. If I vary input signal SDIN (I am using PCM1808 in Master mode (512 fs) with 4.096 MHZ MCLK), there're no visible changes at PWM output.
In case 1) described above I was getting 250 kHz switching at PWM output before; but since I have swapped 4.7nF and 47nF capacitors on PLL_FLTP and PLL_FLTN I have started getting 377.5 Khz.
Thanks,