Hi Don, I hope your well. Im interested in the 5631EVM. It appears to come with '5518 which is an EOL part. Is there a new EVM with an audio processor that is not EOL? Also it appears that the USB input board will accept 192K in via S/PDIF andthe AKM4113. Will the full EVM support all rates from 44-192? I'd like to be able to feed the system 44/48/96/192 without any mucking with the jumpers or software. Will it support this?
Cheers...Doug