Good morning.
I'm using a TAS5706B in a dual mono configuration, so I have two IC for a stereo amplifier.
I use channel A and B in BTL mode.
First question:
can I miss to connect the components to channel C and D.
C and D channel are in shutdown mode during normal working time. In the attached picture you have the current configuration that I'm using without any problem. The idea was to remove at least R16, R19, C69, C77. Could it give a problem?
Second question:
during amplifier stand by I want to reduce power consumption removing 18V voltage, in this way I can disconnect one AC/DC converter. During this time the 3.3V should be still prersent. Could it give some problem to IC the missing of only 18 V power supply?
Thanks for support and BR.
Giulio Grassi