This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sirs,
we are running the PCM2903B AUDIO CODEC chip under WINDOWS XP witout any problems.
Under WINDOWS 7 we now have the problem that ADC input chanels can not be used for recording because the input level can not be controlled.
Is there any solutions for this problem or can you suggest another chip with the same function running under WINDOWS 7?
Kind regards
--
Andreas Richter
General Manager Service
Textechno Herbert Stein GmbH & Co.KG
Dohrweg 65
41066 Moenchengladbach
Germany
Tel: +49 2161 6599-0
Fax: +49 2161 6599-10
http://www.textechno.com
Geschaeftsfuehrer: Dr. Ulrich Moerschel - Kommanditgesellschaft,
Sitz Moenchengladbach, Registergericht Moenchengladbach, HRA 1263
Persoenlich haftende Gesellschafterin: Stein Verwaltungs GmbH,
Sitz Moenchengladbach Registergericht Moenchengladbach, HRB 374
--------------------------------------------------------------------
Product news:
COVAFIL+: Capacitive evenness tester for filament yarns
ITEMAT+: High-speed Interlace tester with interlace stability test
FIBROTEST with extended fibre length measuring range up to 190 mm
Textechno DRAPETEST wins JEC Innovation Award
http://www.textechno.com/drapetest_award
Please visit us at the following exhibitions / events:
http://www.textechno.com/exhibitions
--------------------------------------------------------------------
Hi, Andreas,
Sorry for the delay in getting back to you.
The PCM2903B is NRND according to our website, and the recommended replacement is PCM2903C.
The reason we did that is to fix the exact issue you've seen in Windows 7.
So, if you swap out the B version for the C version, everything will be fine. You can order free samples from our website to verify it for yourself.
-d2
Dear Sirs,
thank you very much for your answer.
I have already maneged to get the C type IC to update our PCB board for further checking.
Kind regards
Andreas