Hello,
I have downloaded TAS570X GED (2.1 build 14). When i start a new design, on the right side, i can select the device. My problem is that only 5707, 5708 or 5709 appear? If i load a default pfw file (TAS5709_10_default.pfw for example), i can change the device to 5709,5710 or 5711! So i'm new to this and completly lost. Do i have the right software? Should i use another device number (similar to 5719)?
BTW, I can connect in I2c w/o problems. I used the I2C memory tool and got "6c" for adress "0x00".
Haven't gone further than that. Would like to know if this is normal or not?
Any help appreciated.