Hello E2Es,
I will be using the DSD1794A in stand-alone mode for some time and would appreciate a tip on how I connect these pins in the meantime:
Pins 1 & 2 (DSDL & DSDR)
Pins 10-14 (ADR0, ADR1, SCL, SDA, RST (reset active low!))
Do I connect them to VDD or to ground (except for reset), and should I add a 10kohm resistor inbetween either VDD or GND?
Tips are appreciated ;-)
Greetings,
Jesper Mønsted