Hi,
Would you perform the following evaluations?
My customer wants a result by this week.
-----------------------
<condition>
・PVcc=24V
・RL=4Ω
・BTL
・Input Wave = Square wave
・Output Wave = Square wave
(The value of THD doesn’t matter)
-----------------------
<result>
・TAS5414B-Q1 Pout(max)=??W @ PVcc=24V , RL=4Ω , Output wave = Square wave
・TAS5611A Pout(max)=??W @ PVcc=24V , RL=4Ω , Output wave = Square wave
* My customer hopes it becomes "Pout(max)=100W @ PVcc=24V, RL=4Ω, Output wave=Square wave".
-----------------------
< back ground >
My customer doesn’t use the Pout(max).
(my customer doesn't drive a speaker in Pout(max).)
However, it is necessary as catalogue specifications of the customer application.
Therefore, it is important TAS5414B-Q1 & TAS5611A can satisfy specifications.
-----------------------
Sorry to ask this of you when you are busy but I appreciate your help.
Regards,
Kanemaru