Hi,
I used CC8521 to make a USB dongle,the hardware works good, but when I used the VOLUME bar(windows xp sp3) to turn down the volume, it didnt work. At last,I found that only the WAVE bar can be used to turn down the volume,as show below:
The SPEAKER bar was gray, it didn't work when value be changed,even though click the first CHECKBOX (Mute) , there was still output. Did I miss any details when I configurate the CC8521? Or anything wrong with my PC operate system? When I plug the dongle,the output always at the MAX volume,are there any configurations to make the OUTPUT at the MIN when plug the dongle ?
Hope for reply, thanks.
Regards.
Jack.