Is it possible to input a Stereo L and R signal into the TAS5706B and use the 7-Band EQ in PBTL mode? The signal needs to be summed within the chip as well.
If yes, then how?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Joseph,
The 7-band EQ can be used in PBTL mode. (note that the device only supports post LC-filter PBTL).
The device does not have a mixer node option to sum L,R signals.
The TAS5706 is a relatively old device, unless 192K Fs rate & closed loop power-stage are key requirements, a newer device would probably work out better. If you can list your application requirements I can shortlist a couple of newer devices for you (with features like pre-filter PBTL & L+R mixing support etc. possible)
-Ravi
Ravi,
The Fs rate is not as important as the closed loop power stage. So it seems that if I want to use this chip I will need to have a signal premixed before entering the device?
We are looking at this chip due to built in 7-band EQ, limiters, closed-loop power stage, 40W-50W total output into 4 ohms.
Any suggestions you have would be helpful.
Thanks,
Joe