Hello,
We've been using the TAS5731 for our projects as of late, taking a hiatus for a few weeks from the amp controls to resolve other project conflicts. When attempting to utilize the amp just yesterday, I noticed a -6dB per octave roll-off starting at about 4kHz, that we've never seen before. After resetting the biquads and disabling the DRC's, we recorded the following identical results from the TAS5731 AND the TAS5711:
The Sub channel has been also displaying a concerning -40dB/decade roll-off at 200 Hz (1st-order 100Hz low-pass). We have double/triple/quadrouple checked where this filter might have possibly been implemented, however there is not evidence of implementation.
After carefully attempting to rewrite the I2C register values through the I2C output window, as well as the Memory Tool, we've noticed that the values we change ARE NOT PERMANENT. Meaning, once the window is closed, then reopened, the default values are restored. We then attempted to run a default process flow in the GDE, only to yield the same response. Our next step was to control the amplifier EVM via a separate computer, with a default process flow, to find an identical response. Our engineering team seems to believe the software (Version 2.1 Build 8) is not capable of highlighting, nor rectifying this behavior.
It is our understanding there is a new TI software that could possibly be available. For your debugging purposes, here's a I2C dump from our chip displaying this behavior:
X05 System control 2 1 40 Write C4
X06 Soft mute 1 00 Write 3F
X07 Master volume 1 FF Write FF
X08 Channel 1 volume 1 30 Write 30
X09 Channel 2 volume 1 30 Write 30
X0A Channel 3 volume 1 30 Write 30
X0E Volume configuration 1 91 Write D1
X10 Modulation limit 1 02 Write 02
X11 IC delay channel 1 1 AC Write AC
X12 IC delay channel 2 1 54 Write 54
X13 IC delay channel 3 1 AC Write AC
X14 IC delay channel 4 1 54 Write 54
X19 PWM channel shutdown group 1 30 Write 30
X1B Oscillator trim 1 00 Write 00
X1C BKND_ERR 1 02 Write 02
X20 Input MUX 4 00 01 77 72 Write 00 01 77 72
X25 PWM MUX 4 01 02 13 45 Write 01 01 32 45
X29 Ch1_BQ[0] 20 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 Write 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X2A Ch1_BQ[1] 20 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 Write 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X2B Ch1_BQ[2] 20 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 Write 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X2C Ch1_BQ[3] 20 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 Write 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X2D Ch1_BQ[4] 20 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 Write 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X2E Ch1_BQ[5] 20 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 Write 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X2F Ch1_BQ[6] 20 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 Write 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X30 Ch2_BQ[0] 20 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 Write 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X31 Ch2_BQ[1] 20 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 Write 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X32 Ch2_BQ[2] 20 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 Write 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X33 Ch2_BQ[3] 20 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 Write 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X34 Ch2_BQ[4] 20 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 Write 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X35 Ch2_BQ[5] 20 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 Write 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X36 Ch2_BQ[6] 20 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 Write 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X39 UNKNOWN 8 00 00 00 00 00 00 00 00 Write 00 00 00 00 00 00 00 00
X3A DRC1: ae, (1-ae) 8 00 7F FF B4 00 00 00 4B Write 00 7F FF B4 00 00 00 4B
X3B DRC1: aa, (1-aa) 8 00 7F FF B4 00 00 00 4B Write 00 7F FF B4 00 00 00 4B
X3C DRC1: ad, (1-ad) 8 00 7F FF B4 00 00 00 4B Write 00 7F FF B4 00 00 00 4B
X3D DRC2: ae, (1-ae) 8 00 7F FF B4 00 00 00 08 Write 00 7F FF B4 00 00 00 08
X3E DRC2: aa, (1-aa) 8 00 7F FF B4 00 00 00 08 Write 00 7F FF B4 00 00 00 08
X3F DRC2: ad, (1-ad) 8 00 7F FF B4 00 00 00 08 Write 00 7F FF B4 00 00 00 08
X40 DRC1-T 4 FC 83 10 D4 Write FC 83 10 D4
X41 DRC1-K 4 0F 83 33 34 Write 0F 83 33 34
X42 DRC1-O 4 00 08 42 10 Write 00 08 42 10
X43 DRC2-T 4 FC 83 10 D4 Write FC 83 10 D4
X44 DRC2-K 4 0F 83 33 34 Write 0F 83 33 34
X45 DRC2-O 4 00 08 42 10 Write 00 08 42 10
X46 DRC Control 4 00 00 00 00 Write 00 00 00 00
X50 Bank switch control 4 00 00 00 00 Write 00 00 00 00
X51 Ch 1 output mixer 12 00 80 00 00 00 00 00 00 00 00 00 00 Write 00 80 00 00 00 00 00 00 00 00 00 00
X52 Ch 2 output mixer 12 00 80 00 00 00 00 00 00 00 00 00 00 Write 00 80 00 00 00 00 00 00 00 00 00 00
X53 Ch 1 input mixer 16 00 80 00 00 00 00 00 00 00 00 00 00 00 80 00 00 Write 00 80 00 00 00 00 00 00 00 00 00 00 00 80 00 00
X54 Ch 2 input mixer 16 00 80 00 00 00 00 00 00 00 00 00 00 00 80 00 00 Write 00 80 00 00 00 00 00 00 00 00 00 00 00 80 00 00
X55 Ch 3 input mixer 12 00 80 00 00 00 00 00 00 00 00 00 00 Write 00 80 00 00 00 00 00 00 00 00 00 00
X56 Output post-scale 4 00 80 00 00 Write 00 80 00 00
X57 Output pre-scale 4 00 02 00 00 Write 00 02 00 00
X58 Ch1_BQ[7] 20 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 Write 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X59 Ch1_BQ[8] 20 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 Write 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X5A Subchannel BQ[0] 20 00 00 05 83 00 00 0B 06 00 00 05 83 00 FB 42 C1 0F 84 A7 33 Write 00 00 05 83 00 00 0B 06 00 00 05 83 00 FB 42 C1 0F 84 A7 33
X5B Subchannel BQ[1] 20 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 Write 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X5C Ch2_BQ[7] 20 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 Write 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X5D Ch2_BQ[8] 20 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 Write 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X5E Pseduo_Ch2 BQ[0] 20 Write 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X5F Pseduo_Ch2 BQ[1] 20 Write 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X60 Channel 4 (sub) output mixer 8 00 00 00 00 00 80 00 00 Write 00 00 00 00 00 80 00 00
Please let me know what the best option to do would be.
Cheers