Hi,
I drive TAS5414A by microprocessor via I2C.
After start all outputs are in a Hi-Z mode.
The load diagnostic function can only be invoked when the output
is in the Hi-Z mode. If the amplifier is already in play mode, it must
Mute and then Hi-Z before the load diagnostic can be performed.
When I set play mode the amplifier is moved out of Hi-Z mode.
How do I go back to HI-Z mode via I2C for load diagnostic ? What is the registry? What is the value ?
Thank you
Peter