Hi
I was wondering if there is a power sequence for the DVDD/PVDD on the TAS5713 or the TAS5727. We are thinking of using the PVDD (18V) rail as the source of our DVDD(3.3V) thus making the PVDD active before the DVDD.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Mike,
This should be okay with the TAS5727. The TAS5713 may pop under this case, but I don't think so. It's an older part, so it's been a while since I played with it.
-d2