I noticed quite strange behaviour during testing my hardware with TAS5707+ARM M4+MEMS mic
Our cell powered device operates from 8.4 to 11V. TAS5707 should operates from 8V, but it has problems to operate properly below 10V! There are sound blackouts when some dynamic or loud sound is played. When the supply is 10V and above there are no problems.
I try to decrease modulation limit from 99.2 to 93.8 and it has effect that the device could play almost without blackouts with supply 9V, but it is far from operate at 8.4V. When I decrease power supply to 8.4V I hear some soft poping in speakers and amplifier isnt working. I must go to 8.7V, the poping disappears but there are big problems with sound blackouts.
My load are two 8Ohm speakers in series and additional 4.4Ohm series resistance as intrinsic safe protection.
Thanks for any help or solution.
Lukas