Hello,
I use a tas5558 with bd modulation (because the outputfilter of my class d amp is designed for bd modulation). Unfortunately there is a high signal noise in bd mode. If I use ad mod. the noise is less noisy, still hearable but quite ok. It doesn't depend on the volume but it dissapears if I mute the tas5558.
Audio source is once a pcm3070 and a dir9001, noise is present at both of them so I think the source is not the reason.
Thanks in advance.
regards
bernhard