This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5611/5613 2xBTL mono from 1 differential input

Other Parts Discussed in Thread: TAS5611, TAS5612LA, TAS5622A, TAS5611A

Hello,

 

I have designed a plateform based on the TAS5611 amplifier chip.

My plateform is done to explore the multiple configurations available from this chip (BTL, PBTL) ; one of our application consists of using this plateform in such a way that we could only have 1 differential mono (L+R) signal inputting the TAS5611 that I want to use in 2xBTL outputting 2 times the same mono signal on 2 dissociated loads.

The question is; is it possible to use the TAS5611, officially in PBTL mode (M3M2M1 = "101" with INPUT_C=1 and INPUT_D=0) inputting my signal using A-B input(differential input) but mapping the output in BTL on 2 loads instead of PBTL (1 load)?

 

Thank you.

 

Antoine.