I am referring to RDK VALUE SB in my soundbar design. I have some doubts in software part.
We are loading the script generated from pure path into EEPROM on the board. At start up all the data from EEPROM is loaded into PCM3070. But srs wow and equilizer are activated only when the buttons are pressed. srs wow is there in the script loaded and it was already loaded into codec, but becoming active only when button is pressed. WHY?
what is happening at power up? is all the data from EEPROM is loaded in pcm or only a part of it is added. then is the remaining registers are writing at run time when button is pressed.
Please explain me clearly what MSP is doing at run time to Registers of CODEC?
Also i want to implement some extra features like head phone out, 3D effect e.t.c .How can I incorporate them in the existing system.
Please do the needful.
Thanking You