hi,
I've read datasheet and user's guide of TAS5713,and here is my confusion:how to balance two band DRC in TAS5713?
we have used TAS5707 and TAS5708 in our hardware board from our project of lab of xidian university,China
And now ,we want to upgrade to TAS5713 to make a better performance in speaker
In TAS5708,there is only one band DRC,and it is easy to learn how to configure it and use it.
But now ,in TAS5713,there are two DRC,upper band DRC and lower band DRC,in one chip.
I have studied your DAP process in TAS5713 datasheet ,and try to understand how it works ,but something in it always confuse me ,and now I still don't know how to configure them to have a better performance compared to TAS5708 using MCU or GDE.
So, do you have something detailed which can tell me how two band DRC works,or can you tell me something which I can according to ?
By the way ,in TAS5708's datasheet ,I know how DRC works.The structure can calculate the gain of audio data and multiply it to the input of DRC.
But in DAP process of TAS5713's datasheet, I just can't get the meaning of input of DRC. It seems like that the input of DRC is output of all DAP ,and the gain of DRC seems not multiply to the input of DRC. Here is the problem .Could you please tell me how it happens?
thank you !!!!
from zhuo yue