This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Which one is better? PCM2704 or PCM2705?

Other Parts Discussed in Thread: PCM2705, PCM2704, PCM2705C

Hello,

I want to build a simple USB sound interface with S-PDIF output. I'm not planning to use an external memory, as I'm content to use the internal USB descriptors. I don't need to use any SPI interface either, neither HID buttons. So, which interface should I be using, PCM2704 or PCM2705? I know I can use both, but which one is simpler to use and requires less terminations/components?

Kind regards, Samuel Lourenço