Hi,
Do you have any products with same function only like the internal line driver of DIT4096?
Could you please tell me if you have?
Best Regards,
Kato
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Kato-san,
You mean something like DRV134?
-d2
Hi Don-san,
Yes, you are correct.
Although I also found DRV134, this device have to be applied +/-4.5V ~ +/-18V as the power supply voltage.
So, could you please tell me the device that is able to be applied 5V like DIT4096?
Best Regards,
Kato
Hi,
For S/PDIF output I use RS485 bus transceiver SN75176B. It has 5V TTL input and 0/5V differential output. This chip can be used also for input. For correct impedance you must add serial resistor (110R for balanced S/PDIF) or voltage divider for unbalanced S/PDIF output. I succesfully used this circuit in my USB DAC:
Hi Pavel-san,
Thank you for your information.
Hi Don-san,
Do you recommend that we use SN75176B that Pavel-san suggests instead of DIT4096 as the line driver for AES-3 encoder?
Best Regards,
Kato