I was trying to fix a Bosch radio for a friend. No schematics or spare parts available (shame on Bosch! ;-). The radio uses a tas5706b in connection with an ADC. All supplies seem OK. ADC input is OK and output looks like decent I2S. SPI signals look OK and are present when volume is changed. But the speakers are dead silent. I can see a small sine wave (probably the modulation freq. from the PWM - at around 380khz (as I remember it). I'm considering trying to change the IC (a pain with the power pad - and I'm afraid to burn the new chip before getting the power pad soldered (only have hot air for one side)). However, I'm a little puzzled that it would burn at all. No signs of thermal overload on the PCB. And according to the datasheet the chip is pretty well protected against almost any probably error... So I'm a bit puzzled why/how it would burn in a system with absolutely no direct external connections!
So the question: What kind of fault modes have you seen out there?
And secondly: Have anyone listened to a tas5706b on a decent stereo setup? Or maybe other similar digital input parts? The features of ie. tas5706b are excellent for an active system - but my previous experiences with Ti PWM amps have not been great. Might be the "lowest possible cost consumer device implementations" that’s not optimal (naturally) - but I'm still a bit reluctant to put in a lot of resources in trying it out.... ;-)
Thanks in advance for your response! :-D