Hi,
I am using the TAS5342a in SE mode to amplify an analog PWM input. I am using only one of the four available channels. At the output of the TAS5342 I only get a DC voltage which is exactly the same as the GVDD voltage, and when I decrease the GVDD voltage below 9.5V (aprox) the output voltage of the TAS5342 it is always 9.5V. Any idea about which could be the problem?
I am following the reference design of the datasheet for Typical SE applictions.
Thank you very much in advance