HI
I'm using the GUI for the eval board TAS5342DVV6EVM version 4.0 RevA. I'm having issues with the volume control, it does not adjust. Nothing comes out until the input hits a certain level and I get max volume. The volume control seems to adjust the threshold level. I'm certain the volume worked like a volume control before, being able to set the input and adjust the output. So I believe I changed something and I have not been able to figure out what that was.
FYI, I have been running the GUI on Windows 7 and XP with no difference in preformance. Everything seems to be fine,
I would appreciate any help, I have a presentation of the system design coming up and its a bit loud. To compensate I turn the input source way down but then it's close to the noise floor and you hear the niose well.
Thanks
Tom H.