Are there any specs for the inductors on the TAS5414A output channels?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Are there any specs for the inductors on the TAS5414A output channels?
The requirements for the inductors will vary by application. For a standard 2 ohm or 4 ohm application we use a filter with a 10uH, dual core inductor. The inductor should be capable of handling 3 - 10 A rms depending on the application.
The EVMs use the TOKO HEAW inductor. This particular inductor is AEC-Q200 (automotive) qualified. The specs on this device are very similar to the TOKO EAW family of inductors.
Another similar inductor is made by a company called Sagami - I am not as familiar with their products, but I believe the DBE1010 line of products are very comparable to the TOKO devices.
-Aaron