Dear Sirs,
My Customer asked to me about differences between TAS5XX and TAS5548(Pure Path Console).
When the following conditions start the GUI not in check in each set after I2C Logging settings DRC_1 the data had different as follows.
Please tell us about this difference.
GUI EVM ADRESS RESISTER THRESHOLD DATA
TAS5508 - 0x99 DRC_T1 -100dB 08 4E 08 B2
TAS55xx_GUI TAS5624AEVM 0X99 DRC_T1 -100dB 0A 55 55 55
PPC TAS5548EVM 0x99 DRC_T1 -100dB 08 4E 08 B1
TAS5508 - 0x99 DRC_T1 -58.66dB 04 DF 21 AC
TAS55xx_GUI TAS5624AEVM 0X99 DRC_T1 -58.66dB 06 E3 69 D0
PPC TAS5548EVM 0x99 DRC_T1 -100dB 04 DF 21 AB
Also, please tell me TAS5548 of GUI (PPC) can be used in EVM of TAS5624A. (The latest of Userguide is equipped with TAS5558)
TAS5624AEVM of GUI (TAS55XX), please tell me if you can use in EVM of TAS5548. (USB communication was OK)
Best Regards、
Y.HASEBE