Hello,
Customer is looking for a low cost, mono, analog in, class D amp that will deliver 3W@1% THD+N, 4 ohm load with a 5 V supply. Adjustabe gain would be nice but not a must. I suggested the TPA2038D1 but it comes up short on power at 1% THD. Any suggestions for another device or a digital input device that might get there?
If they switch to 8 ohm load it looks like the TAS2553 would work. Any others?