Could TAS5713 and AIC3254 perform separate bass/treble volume change?
Also, could AIC3254 output analog and I2S signal simultaneously?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Could TAS5713 and AIC3254 perform separate bass/treble volume change?
Also, could AIC3254 output analog and I2S signal simultaneously?
Thanks.
Hi Terence,
Welcome to E2E, thanks for your interest in our products!,
The TAS5713 features two DRC in series configuration, this allows the device to limit the output of two different previously filtered signals and act as a crossover. You can use this function to limit the output of the bass and treble frequencies.
Effectively, the AIC3254 is able to output I2S and analog signal simultaneously.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer
Can AIC3254 also limit the output of bass and treble frequencies?
Is it possible to change the output of bass and treble frequencies in real time, for example, changing with the volume knob?
Many thanks.