Hello!
On Friday, the 23rd April, i got the TAS3308EVM-LC Board.
This Weekend i tried to work with the Board.
I load in to the I2C Command Tool the 3308_init_master configuration script and make all the first steps, that are discribed in the User Guide of the board.
Then i load the TAS3308 Example Process Flow and at the Headphone i hear nothing.
For project i want only use the PWM Outputs.
I thought i made something wrong so i make a really easy Process flow. I just connect a ADCIn_1 with a PWM Out and hear also nothing.
In the Probe Point Window i see the signal, that came through the line in, in all Points. So i think the TAS get the signal but the outputs make nothing.
Have i do some configuration i don't know?
Now i hope someone can help me.
Greeting, Markus