This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5706B, TAS5716 vs. Newer Models

Other Parts Discussed in Thread: TAS5706B, TAS5716, TAS5756M, TAS5754M

I've used both the TAS5706B and TAS5716 in the past with excellent results. Is one of them still the best choice today? I want audio fidelity specs equal to or better than the TAS5706B/TAS5716. Here are my other requirements:

*  Minimum of 2 channels x 20 Watts (<1%THD) into 8 Ohms or 4 Ohms (I can get the speakers in either impedance)

*  I2S input @ 48kHz sampling rate

*  DRC

I won't be using headphone or subwoofer outputs, volume control, EQ, Pseudo-Bass.

Any suggestions?