Hi,
It's indicated on a datasheet as follows about the Shutdown voltage of LM4674.
<Datasheet P.5>
Shutdown Voltage Input High : VSDIH=1.4V(min)
Shutdown Voltage Input Low : VSDIL=0.4V(max)
(VDD = 3.6V)
When using by 5V(VDD), is this spec same?
Regards,
itabi