Team,
I have a few questions about the TAS5414C-Q1 device when using the SYNC signal.
- 1. What would happen to the TAS device, while operating with a SYNC input, if we intermittently lost the SYNC input signal and then got it back again?
- If it we in the millisecond range, what would be the results of this event? The reason being that the uC supplying the SYNC went through a reset period.
- 2. What would happen to the TAS device if the SYNC input received a constant logic high?
- 3. What would happen to the TAS device if the SYNC input received a constant logic low?
- 4. What are the limitations of the SYNC input if you wanted to change frequencies on the fly for AM avoidance using the SYNC input?
- Could you just step the Frequencies or is there a limit on the amount of time in which you can change this SYNC frequency?
Thank you,