Hello,
I need to capture 16 differential audio channels and transmit them in a single bus (an FPGA will read that bus). I think TLV320AIC14K is perfect since I can cascade 16 ICs so that I get the 16 channels in a single bus by using the SmartTDM feature.
However I need to remove a non-desired component at 2280Hz (which is line signalling that has to be hardware removed). Since 2280Hz is within the audio BW I thought of a notch filter before each TLV320AIC14K CODEC.
How can I proceed which the notch filter? a switched capacitor filter? an op-amp IC? (I need a very selective filter).
I also realized that other CODECs can notch filter such us PCM1870A but they don't have SmartTDM feature (and it is very convenient for me).
Many thanks for your help in advance