Could you please take a look at the following questions about the TAS5711EVM and help me answer them for the customer:
I've been digging into the TAS5711EVM kit to see if it can be used to help us do a quick evaluation of the loudness of the speakers we are proposing to use in the Hurricane demo. I have a few questions, but I'm not sure which of you to ask, so I've copied everyone.
1) Is there a newer version of the TAS5711EVM users guide than the one on the TI web site I've downloaded the GUI software and noticed that there a number of inconsistencies in the users guide relative to what the GUI presents?
2) Is there a configuration file that sets up the EVM kit to simply put the EVM in 2.1 mode and pass signals from the LIN/RIN (analog) connectors to the speakers with or without any equalization etc.?
3) What is the difference between the TAS5711 and TAS5713? From a quick look at the datasheets, it appears that the TAS5713 is intended for driving lower impedance loads, but has a recommended PVDD of 21.5 rather than 26V.
Thank you very much for your help!
Joe