Hi,
1. I currently use the TAS5602, but I found that the Crosstalk value would be changed with different PVDD level. Is it correct?
The best case is same as datasheet when PVDD is 16v~19v. But after the PVDD over 20v, the value will drop to 60dB.
2. I'm also looking for AMP to meet below spec, could you provide some ideal. That will be good to with the reference prices.
- SNR>98dB
- Crosstalk> 60dB
- PWM input /
- 2x25W-30W BTL output with 6ohm
- PVDD 20V
Thanks