I am looking for a class-d solution with PWM input (be generated by a µP)
that can work with very low frequencies ,even DC.
Is that possible with the TAS5612a or is he going to block DC?
I don't need a lot of power, the modified speaker is 6 Ohm DC and I need maximum 1.2A.
Frequentie from 0Hz (DC) to 5Khz.
I use the modified speaker as air pressure control valve in an organ.