This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sirs
I use PCM2912 to buin test.
For BurnIn Test, =>”Failed to play back MIDI via sequencer” issue,
Could you have any suggestion? Thanks
Audio IC PCM2912: inbox driver,
OS: Win7_64bit,
CPU: Intel Broadwell-DE D-1559
BRS
Nat
Dear Ivan
I test PCM2912A.
Thank you for your support.
I have two question:
1.How long do you test MIDI play back function?
I test it one more hours and fail 2~3 cycle.
2.Is it the Compliance issue? (My CPU is Intel Broadwell-DE D-1559.)
BRS
Nat
Nat,
The complete test takes around 15 minutes. The MIDI file is played for 5.5 Sec each cycle.
There is no precedent of compliance issue other than what is explained in PCM2912 Errata but I will do some research to see if I find some similar issues.
Best regards,
-Ivan Salazar
Texas Instruments