Other Parts Discussed in Thread: NE5534
Hello,
I have a new design that I have been trying to test. However, the TPA3116 is going into immediate fault when it is powered on. Here are the troubleshooting steps that I have performed so far:
- Check short between all outputs and POSITIVE power input
- Check short between all outputs and GND
- Check for shorts between output pins
- Check for shorts between POSITIVE power input and GND
- Check for shorts between each and every pin on the IC.
- Obviously SDZ and FAULT are tied together
- PLIMIT and GVDD are also tied together
- Use oscilloscope to watch the FAULT pin
- The IC is not resetting itself. Once the chip is powered on, FAULTZ goes low (I'm reading 0.59 Volts on this pin) it goes into immediate fault and does not recover. I can watch the scope and you can see fault go high as the battery is plugged in, but immediately goes low and stays that way.
- Use oscilloscope to watch for DC offset on the outputs
- I'm not seeing any DC offset at all when the chip is powered on. It goes into fault far too quickly to get a reading here
- Use multimeter to watch for over current condition
- I don't think my multimeter would read this accurately anyway. Once the battery is plugged in it goes into immediate fault and the first current reading I get is the quiescent current (around 0.3mA MAX)
Here is my setup:
- Test board
- Battery Powered: 11.1V Lithium battery with 80A continuous discharge and 160A burst discharge.
- 6 ohm speakers
- 26dB Gain setting (100K and 20K gain resistors)
- 1uF input caps
- Single-ended input (can see how I do that in the schematic) using a 3.5mm headphone jack
Here are the images of the schematic and the board: