Hello Audio Folks, a customer is asking the TAS5707 internal precision. I know the max db is 24db. So, what is the min db level? and what is the resolution (i.e. number of bits used)?
Regards,
Kes
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Kes,
Are you referring to the precision of the volume of the amplifier?, if so, the max dB is effectively 24dB, and the minimum is -79dB.
I would like to add that this device is quite old, and we have newer devices with enhanced processing, better overall performance, easier end-system integration and reduced cost compared with the TAS5707, like our TAS5751M and TAS5733L.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer