I am working with a PurePath Console Motherboard AIP005F and TAS5751MEVM which
were acquired about a month ago. I just downloaded and installed PurePath
Console 3 which went fine. However the list of "Available EVM Apps" after I
sign in only shows "I2C Master" which I installed.
I'm logged in and have a license for PPC3. There is no indication in the PPC3
documentaion that TAS5751 requires an additional license. And it IS listed as
being supported by PPC3 (and only PPC3). Also the motherboard is plugged into
USB, the TAS57521MEVM is plugged onto the motherboard, a 24V power supply is
attached, and all of the proper LEDs are illuminated.
So how do I get the "Available EVM Apps" populated with TAS5751MEVM (or anything else) so I can
install it and get moving?
HAL