Hi
I am having some problems in muting the TAS3308 with external HW control through the mute pin.
The description of the IIC mute control register 0x09 is indicating that the default value with mute(1:0) = 00 should be external HW mute control but despite that the TAS3308 can't be controlled, it is playing at all times despite the level of the mute pin input.
The mute control register documentation is not very good - it doesn't contain any information on where the mute control bits are in the 4 bytes the register consist of :-)
So I hope someone can help me in muting the device,
best regards
Jes Mosgaard