Hi
We have question about the overcurrent limit protection of TAS5342LA.
We can refer the following description on the datasheet.
IOC=8.4A(typ)
Resistor-programmable, high-end, ROC=22Kohm with 1ms pulse, Tc=75C
Questions.
1. How to consider IOC limit?
For example,
Speaker load=4ohm, PVDD=32V, BTL:
How to obtain the current that should be limited?
And what Roc value is a reasonable?
Could you please show me an example?
2. What is the meaning of "with 1ms pulse"?
BestRegards