This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI experts,
I have some questions about PCM5102A as below, I appreciate your help.
Fai~
In my system, there are different audio signal input to the system and using PCM5102A is an analog output terminal for headphone.
Case 1: PC's headphone(SE) signal output to (ADC)PCM1861 without gain to generate I2S signal to the Amp & (DAC)PCM5102A.
Question 1 : The Vrms from PC is 1.3V, and 5102A's output Vrms is 1.2xV, so there is about 0.05V ~ 0.1V different. is it normal ? or is 5102A supposed to generate the exact same Vrms level as the original level from PC ?
Question 2 : Are the below scenarios caused by the LowPassFilter or the Anti-aliasingFilter or other reasons?. I want to reconstruct the analog signal precisely from 5102A which can (1) have same loudness as the original signal from PC. (2) maintain a clean signal in full range frequency.
Case 2: Using TI's USB-I2X board connected to PC as a soundcard to generate the I2S signal to PCM5102A
Question 1: same scenarios and results happen as above Case 1's question 2_scenario A and B
*** The anti aliasing filter to PCM1861 and the circuit of PCM5102A (with LowPassFilter) is show as below.
*** The signal is shown as below ( Top is the original signal ) , (Middle is after 5102A with LowPassFilter) , ( Botton is after 5102A without LowPassFilter )