Other Parts Discussed in Thread: PCM5102,
Tool/software:
I want to use I2S to generate audio through PCM5102 and switch 4 channels using CD4052.
I want to select 4 speakers through the control of the MCU and output them to 1 speaker. (Not more than 1 speaker output at the same time.)
Would it be desirable to switch the output through de-mux using one PCM5102A as shown in the figure?
Or should I control the Input I2S signal using de-mux using each of the 4 PCM5102A as in case 2?
Please give me some advice.
Regards,