We are having a problem with either of these 2 SPDIF TX chips. If the COPY and GENERATION (L) bits are set to "Pro", some Crystal RX chips read the wrong TX frequency. If the bits are set to any of the "Consumer" modes, the old Yamaha RX chip read the wrong frequency info.
Yes, aside from the fact the frequency read-out is wrong, they work. But, some of our customer's units need that frequency info, in order to switch in the right VCXO. (Yes, most don't have a secondary VCXO. It might only be 1% or so, but this problem has to be solved.)
Not that it matters, but I am sure someone will ask:
System clock is 11.2896 MHz. L/R clock is (obviously) 44.1 kHz. Operating in h/w mode. And, yes, the validity bit is set right, or none of our customers units would work.
Anyone want to guess what is wrong?