1 I use TAS5717 THD+N=1%,.12V power supply, 6 ohm speaker, now that the speaker output voltage is only 3.1V, I want to make the 8W sound, when the output voltage increases, there is the distortion of the situation, how do I do now?
in addition
2 I would like to do stereo to mono, both in the AB channel output, how should be configured
3 I only use the AB channel, then I am in the design of the circuit, it should be how to design the CD channel, directly suspended?