Part Number: PCM2707
Before committing to more elaborate designs, I'm trying to give it a quick try. In particular, I want to see if there are any surprises with Linux recognizing the device (mostly interested in Ubuntu).
If I want to start by just to seeing the device appear on the "Sound Settings" dialog, regardless of being able to hear the actual sound, I guess that the absolutely minimal setup would be just connecting the 12MHz crystal and the four USB pins to the corresponding four pins in the PCM2707? (that would be: Vbus to pin 24, D+ to pin 23, D- to pin 22, GND connected to pin 20 -- DGND)
Literally, just that --- *all* of the other pins unconnected. Should this activate the USB device and show up in the host's "Sound Settings" dialog? (again, my question is not: does this work well? the question is: should this work at all?)
I just tried it and it's not showing up on the Ubuntu 14.04 "Sound Settings" dialog. (disclaimer: I know I could simply try adding the missing components and connections and see; but the prototype setup makes it a bit hard to solder in components, so I figured I'd ask for some hints/pointers to help me minimize changes for a quick test)
Thanks,
Carlos
--