This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Do we have solution to support two digital mic and stereo line-in in the same time?
Can ADC3101 support this request?
Thanks,
SHH
Thanks for your help Art!,
Hi, Scott,
The TLV320ADC3101 can support up to two digital microphone inputs, however, it is not possible to operate this part with the two digital microphone inputs enabled and a stereo line input at the same time.
I would recommend you to take a look to the PCM18604 or PCM1865, these devices support up to four digital microphones and have a digital mixer capable of perform signal mixing between stereo digital mics and stereo line inputs.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer
Hi Diego,
Customer would not like to mix the digital mic and line-in signals.
Could PCM8164 capture the PDM digital mic, stereo line-in and output TDM format without mixing the digital mic and line-in signals?
Thanks,
SHH
Hi, Scott,
Thanks for the feedback. The PCM1864 is able to stream both analog and digital mic inputs at the same time in TDM format without mixing the signals. This can be configured in Register 12.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer
Hi, Scott,
For customer's use case, the option would be 01: 4ch TDM. The PCM1864 should be configured in TDM mode, then the device will stream four channels of data. DOUT2 is optional. The data for each channel (Ch1 or Ch2) can be selected using the digital mixing function of the device. As example, you can configure the mixers as follows to stream two channels of digital mic and two channels of analog in data:
01 4ch TDM:
DOUT1: Left Line (Ch1L), Right Line (Ch2L), Left Dmic (Ch1R), Right Dmic (Ch2R).
Best Regards,
-Diego Meléndez López
Audio Applications Engineer