My set up is as below:
Vin and GND- 5V input
PVCC and GND 9V input, shutdown off, mute off and volume turned to MAX.
Lin- 1Vpp sine wave from Function Generator, JP2 shorted, JP4 connected to ADC , USB powered from PC, Speaker of 4 ohm connected across Left output of evm. all the clock jumpers are connected.
i see I2C read values from registers as 00, (0x1b, 0x50 etc) . we are not able to hear any audio output. Please help