Other Parts Discussed in Thread: TPA3140D2
Dear Sirs,
My customer asked us about the resistance of the voltage divider of GVDD for TPA3144D2.
The following description is on page 12 of the data sheet of TPA3144D2.
”The resistance of the voltage divider should be a minimum of 100 kΩ in order not
to overload the GVDD regulator of TPA3144D2.”
On the other hand, the following description is on page 17 of the data sheet.
Under the condition of PVCC = 12 V and RL = 4 Ω
Voltage dividing resistance value is 90 kΩ and less than 100 kΩ.
Please tell me the correct value (description)?
Best Regards,
Y.Hasebe